Dear Team,
I have a custom board with AM335x using Dual Ethernet Support, and using phy device LAN8710 SMSC Device.
Ethernet Interface 1 connected in RMII Mode
Ethernet Interface connected in MII Mode
RMII Phy Address is set to 0:00 in hardware.
MII Phy Address is set to 0:03 in hardware.
When the board boots up, during ethernet phy scans, its detecting the Phy 0 & 3 and its up and run without and issues. but, when i do a soft reset, (reset button)
after the board reset, from the console we find Phy address 0:03 changes to 0:02, this will happens only when soft reset, if we done a power recycle, phy address will stay as 0:03.
Please help me to resolve this issue.
Regards
Jithin