Hi All,
I am trying to convert CCS3.3(DSP/BIOS) project into a CCS5.2(SYS/BIOS) project.
In DSP/BIOS program(CCS 3.3), there is BUFFER MANAGER MODULE, and under that EVENT BUFFER is configured STATICALLY. Now i need to configure the BUFFER MANAGER MODULE in CCS 5.2 statically,but there is no such module available in CCS 5.2. how can i find it?
The following statement is used in the DSP/BIOS program :
BUF_free(&MYBuffer, DataPkt);
But if i use the same for CCS5.2 i get the following errors
Error given was : BUF_free is undefined,MYBuffer is undefined.
please help me to configure this BUFFER MANAGER satatically in CCS 5.2.