This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Value of AM335x GPMC_Config7_0 register during XIP Boot

Guru 15520 points

Hi,

I have a question about AM335x ROM Bootloader.

If we select "Address/Data Mux XIP Boot Mode",
what value will be set to the GPMC_Config7_0 register by ROM BootLoader?

When we boot the ICE from NOR Flash,
the GPMC_Config7_0 register's value was 0x00000F48.
Is this the value which ROM BooLoader set during boot?
MASKADDRESS : Chip-select size of 16MByte
BASEADDRESS : 0x0800 0000 which correspond to NOR address 0x000 0000

best regards,
g.f.