This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

reconfiging usb , then stoped



when i config usb in bootloader, it's works well .The configuration is as following:

         /* Initializing the ARM Interrupt Controller. */
    IntAINTCInit();
         /* Enabling IRQ in CPSR of ARM processor. */
    IntMasterIRQEnable();

        // config the USB module.
    // USB module clock enable
    USB0ModuleClkConfig();
    /* Configuring AINTC to receive USB0 interrupts. */
    USB0AINTCConfigure();
    // UPD Pin setup
    UPDNPinControl();

        /* NAND Pin mux and clock setting */
    NANDPinMuxSetup();
    GPMCClkConfig();
    EDMAModuleClkConfig();

        //Delay timer setup
    DelayTimerSetup();
    enableModuleClock(CLK_TIMER7);

        /* Enable the WDT clocks */
    WatchdogTimer1ModuleClkConfig();
        /* Reset the Watchdog Timer */
    WatchdogTimerReset(SOC_WDT_1_REGS);
        /* Disable the Watchdog timer */
    WatchdogTimerDisable(SOC_WDT_1_REGS);
        /* Perform the initial settings for the Watchdog Timer */
    WatchdogTimerSetUp();             

    // Initialize the transmit and receive buffers.
    USBBufferInit((tUSBBuffer *)&g_sTxBuffer);
    USBBufferInit((tUSBBuffer *)&g_sRxBuffer);

    // Pass our device information to the USB library and place the device
    // on the bus.
    USBDBulkInit(0, (tUSBDBulkDevice *)&g_sBulkDevice);

--------------------------------------------------------------------------------

but when i reconfig it in my os , just aften run into the main, it stops where i enable the usb interrupt.

the configuration is just the same as that in the bootloader.

Can anyone help out of this problem ?