This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Blackhawk USB560M to 5510



I have a generic JTAG connection to a TMS320C5510 situated on a proprietary hardware radio. I am trying to connect a USB560M to this device. It passes the connection scan test, but when I try to connect I get a message that the processor is being held in reset.

I am using CCS 5.3. This version has a pre-installed driver for the USB560M -> C5510 which I have activated and which, as i noted, passes the scan test.

Still, when I try to connect to a dsp which is clearly out of reset and generating debug messages via ipc I get the processor in reset message.

Is there some setting I should be looking at?