Hi,
I'm using TPS65910AA1 to power AM3357. The PMIC's PWRHOLD is connected from processor's PMIC_POWER_EN signal, and the PMIC's PWRON is connected to a button witch. We found that once the power is supplied to the board, without pressing the button to trig one PWRON Low event, the PMIC automatically powers up the processor. I just like to know if PWRON can be used to control TPS65910AA1 power. I saw there is a graph in the fig.5 of the datasheet, but I don't know if it applicable to TPS65910AA1 too.
Thanks,