This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

increase the number of capture buffers

Other Parts Discussed in Thread: DM385

Hi all,

SW: IPNC_RDK_V3.2
HW: DM385

Below params. is defined and used for creating capture buffers.
#define CAMERA_LINK_FRAMES_PER_CH_HIGH_RESOLUTION 6 (cameraLinkPriv.h)

I tried modifying this value from 6 to 4/10/12/24/ etc... If num. of buffs.  decreased below 6(ex:4) system work fine.

In case if I increase it above 6(ex: 12/24) etc, system asserts in one or the other part.Hope memory is not a constraint, because memAlloc() is succesfull, but run time assertion is observed after processing few frames.

 Basically I want to increase number of capture buffers fro  6/8  to as high  as 64...!!   IS that possible?

Appreciate your help.