This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

GPIO



Hi

presently i am working on 816x/393x spectral digital board. I am not able to identiy between the two GPIO present on the board . i have gone through the schematic diagram and datasheet . i am able to know the name of the address register but not there application. I have seen the POST in which JP2 on the daughter board is used for the general purpose input and output. but i am unable to find which bank of GPIO is interface as JP1 is only 20 PIN.

any link or documentation regarding the usage of JP2 AS GPIO and how the GPIO PIN ARE INTERFACE TO THE DAUGHTER CARD would be of great help .

PLEASE HELP ME OUT

  • Hello,

    Check the following documents:

    http://support.spectrumdigital.com/boards/evm816x/reve/ - C6A816x/AM389x EVM Board schematics (PDF)

    http://support.spectrumdigital.com/boards/evm816xiodc/revc/ - DM816x/C6A816x/AM389x Expansion I/O Daughter Card schematics (PDF)

    The JP2 input/output expander is interfaced with the GPIO0 and GPIO1:

    gp0[27]

    gp0[26]

    alt_gp1[15] which correspond to gp0[29]

    alt_gp1[14] which correspond to gp0[21]

    alt_gp1[13] which correspond to spi_scs[1]

    alt_gp1[9] which correspond to gp0[23]

    gp1[12]

    gp0[24]

    BR

    Pavel

  • hi Pavel

    thanks i am able to change the value on the gpio pin using sysfs entries.