This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

aintc module access from a9 4430/60

Good morning,

I search almost all documents for the aintc base address when accessing from mpu A9 but I can't find this address, or how to set-up the aintc module from A9 core.

Does anyone know this address or how to access the aintc registers from A9 core?

thank you in advance.

Best regards.

  • The term AINTC is used in AM35xx/OMAP-L13x and other TI''s processors, for these one reference link is

    http://processors.wiki.ti.com/index.php/Configuring_GPIO_Interrupts.

    In OMAP you can find this information in chapters "4 Dual Cortex-A9 MPU Subsystem" and "17 Interrupt Controllers" (see 17.4.1) for OMAP4430/OMAP4460 TRM (Technical Reference Manual) that can be downloaded from User's Guide section in

    http://www.ti.com/product/omap4430

  • Hi Manuel

    I see this information but I don't see details of registers, how to use the interrupt controller.

    I look to linux source code , the interrupt module is almost the same like interrupt controller from AM335x(seeing the structure of registers), for this reason I copied the driver from AM335x to omap4 but if I don't know the registry structure of interrupt module and details about these registers I can not create a driver for this module, without this module I cannot use almost all interfaces, like DISPC, MMC/SD etc, the same problem I have with the PL310 cache controller and the MMU for the A9 cores, no details, the TRM is direct me to infocenter.arm.com/help/index.jsp but on this site i find only general information, nothing useful to create a driver.

    If I look on linux source code for these information I think that I finish every driver in about one year. And this is not good for a developer.

    I work to a sdk for omap4 like StarterWare to create standalone applications, for now I created the GPIO, UART and I2C drivers and apy's, but here I stuck because I need a interrupt driver, and a DMA driver.

    Best regards.

  • Yes, I just reviewed what you mentioned, and all the information related is redirected to ARM site.

    PL310 information

    infocenter.arm.com/help/topic/com.arm.doc.ddi0246b/DDI0246B_l2cc_pl310_r1p0_trm.pdf

    Cortex A9 Interrupt

    I couldn't find a pdf for this documentation.

    infocenter.arm.com/help/topic/com.arm.doc.ddi0388-/

    I am not sure if adding direct links could affect, I don't know if the spider or web search engines could be affected, if that is the case please mention it in order to remove the links and just mention the filenames, I am not sure if there is some agreement to read the files I just search for them in general search.

    There is only one reference to "Table 17-2 shows the Cortex-A9 MPU INTC interrupt mapping." that I thought was the register information.

  • Thank you very much, in "DDI0246B_l2cc_pl310_r1p0_trm.pdf" is explained everything about PL310 controller.

    Now I have another problem.

    The PL310 has some registers that can be write in secure mode.

    About this I understand that the MPU to be able to modify secured registers, is necessary to put the MPU in secure mode.

    In debug mode I look to base address if is correct and the base address of PL3310 is correct, I can see all data inside PL310 registers.

    After calling a function to modify a secured register i put the controller in secure mode but the controller go to "Data abort" when the MPU try to write in a secured register from PL310.

    this is an example:

        asm("    MSR   cpsr_c, #0x13|0xC0");


        pl310->pl310_clean_inv_way = 0xFFFF;//Non secured register
        pl310->pl310_intr_clear = 0xFFFF;//Non secured register
        pl310->pl310_ctrl |= pl310_ctrl_cache_enable;//Secured register
        CPUSwitchToUserMode();

    When try to write to "pl310->pl310_ctrl" go to "Data abort".

    Best regards.

  • About secured procedures, the information about it is Under NDA then it is recommended to contact a TI representative and check what information is available.

    Suggestion, try to create a new post for each different topic.