I have a dvs8168, I run the demo:dvr_rdk_demo_mcfw_api.out , and select my h264 file to decode, but it cannot decode the file.
help ! can you get my a h264 file???
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can you share the .h264 file that is not playing. Which DVR RDK version are you using. You can find a h264 file of 1080P resolution at this link.:
https://docs.google.com/open?id=0B0699GGnR-MpNWFDaTBPVzJtdjQ
The ini file should be
[file00]
path = dm816x_1080p_demo.264
width = 1920
height = 1080
enable = 1
codec = h264
numbuf = 0
displaydelay = 0
Hi Badri,
thanks for your reply. I am using the DVR RDK version DVRRDK_02.00.00.23. And the decoded file is saved from DM368 encoder, using the API (get_avdata & SaveVideoFile) of APPRO solution .
could you get the h264 file that can not be decoded from this link:
http://l17.yunpan.cn/lk/Q2sgtq3ZwUB5S
thank you
Hi Badri, thanks for your reply. I am using the DVR RDK version DVRRDK_02.00.00.23. And the decoded file is saved from DM368 encoder, using the API (get_avdata & SaveVideoFile) of APPRO solution . could you get the h264 file that can not be decoded from this link: http://l17.yunpan.cn/lk/Q2sgtq3ZwUB5S thank you