Hello,
I'm using the C6748 LCDK and want to run a few audio processing examples. I'm very new to the kit.
Could someone point me to where I could get example projects for the C6748 for audio-passthrough?
Akshay
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'm using the C6748 LCDK and want to run a few audio processing examples. I'm very new to the kit.
Could someone point me to where I could get example projects for the C6748 for audio-passthrough?
Akshay
Hi Akshay,
starter examples of McASP which demonstrates audio input and output in I2S mode using DMA are available.
You can try running those examples.
Download the starterware-c6748 from this link: http://www.ti.com/tool/starterware-c6dsp
After installation of starter-ware, you will find the McASP examples under "../../C6748_StarterWare_x_xx_xx_xx\examples\lcdkC6748\mcas"
You will also find the following links useful:
http://processors.wiki.ti.com/index.php/StarterWare_01.20.01.01_User_Guide#McASP
http://processors.wiki.ti.com/index.php/StarterWare_Audio_Application
Regards,
Shankari
---------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.
---------------------------------------------------------------------------------