Other Parts Discussed in Thread: AM3892
Hi,
I have custom board based on am3892, i'm trying to run Android but during boot 'recovery' is called. Have you got any clues about this issue?
Here I provide full log:
Terminal log file
Date: 04.02.2013 - 8:43:28
-----------------------------------------------
я
U-Boot 2010.06 (Feb 01 2013 - 15:06:53)
DRAM: 2 GiB
Using default environment
Hit any key to stop autoboot: 0
mmc1 is available
reading u-boot.bin
180416 bytes read
## Starting application at 0x80800000 ...
U-Boot 2010.06 (Feb 01 2013 - 15:13:21)
TI8168-GP rev 1.2
ARM clk: 987MHz
DDR clk: 398MHz
I2C: ready
DRAM: 2 GiB
NAND: HW ECC Hamming Code selected
NAND device: Manufacturer ID: 0xec, Chip ID: 0xdc (Samsung NAND 512MiB 3,3V 8-bit)
NAND bus width 16 instead 8 bit
No NAND device found!!!
0 MiB
*** Warning - bad CRC or NAND, using default environment
:,;;:;:;;;;;;;;r;;:,;;:;:;;;;;;;;:,;;:;:;;;;;;;;:,;;:;:;;;;;;;;:;;;;;;;;:,;;:;:
;,;:::;;;;r;;;rssiSiS552X5252525259GX2X9hX9X9XX2325S55252i5:,;;:;:;;;;;;;;:,;;:
;:;;;;;;;rrssSsS52S22h52299GGAAMHMM#BBH#B#HMM#HMBA&&XX2255S2S5Si:,;;:;:;;;;;;;;
;:;;r;;rsrrriiXS5S329&A&MH#BMB#A&9XXA252GXiSXX39AAMMMBB&G22S5i2SSiiiisi:,;;:;:;
;;;;;r;rr2iisiih393HB#B#AA99i22irrrX3X52AGsisss2Xii2299HBMA&X2S5S5iSiisSsi:,;;:
r:r;rrsrsihXSi2&##MHB&Ahh3AGHGA9G9h&#H##@@@##MAMMXXX9SSS29&&HGGX2i5iisiiisisi:,
;;rrrrsSiiiA&ABH&A9GAGhAhBAMHA9HM@@@@@@@@@@@@@@@@@@@HHhAh2S2SX9&Gh22SSiisiiisii
r:rrssisiS2XM##&h3AGAX&3GG3Ssr5H@M#HM2; ;2X&&&MHMB###GBB#B&XXSSs529XX55iSsisisi
r;rsrisSi2XHAhX99A3XXG&&XS;:,rH#HGhAS @@@@3rs2XBM@@A552&&AHA2XiisSS252SSsisSs
r;issi5S22&&3iSSX292&hXsr;;:;h@&G339&S9@@@@2@MA&9&HB##Xris29ABMAAX2ir;rsSi5iss5
rrsSi2XhG&9GXh399&X99i;;;;;;r#H&293H9X#@@@@@@@B&9GhAH@XrrsrsiXABHB&HG2rr;rrSiSi
;:rsisS599&AA9XG&3A35r;:::;,;BMh&&2iX5A@@@@@@@&392X5GB2;;;r;iSX393A##A&Xi:::rsi
;:rss552222X553&XHMhir;;::,:,h#HhGSXhG3#@@@@#AXXS2XAHA;::;;;;ss55XShBA3239r:,;;
r;ii2S5SSi2i53hirsh2srr::,,,,;MMXX359&Ah3h&Si59SX99A#i:,::::;;sri2,.2r;:SGAr;,:
;:;rrrrssiriXGSi::shs;;;,,,:,,rBBA9h5s5h5iS5isi2SAHB5:,,,:::;rrs5&SrisSX5Srrr:,
;,r;;;;rsriSSrrrr;;5Xrr;;,:,,.,;9AA2SsisS5323XXXG9&i:.,,::;;r;;;srrrrrr;;:;::::
:,;r;r;rrissrrr;:;::;s;;;;,:,,..,r293h222hXXAAGGGX;:,,,:,:,::;:;::,:,,,,...,,,,
;,;;;;rrrrrrrrirr;,.,,:::::::,,,,.,;SX&ABAB2hhXir:,,.,,.,,:,,,,..,,,..,..,,,..:
:.:;:;;;:;;;;r;rrs;:.. ,,:::::,:,:,,.::rrsrr;;,,.......,..,....,,,,,,,...,.,,:,
:.:::,::::::;;r;rrr;:.......,.,.,,:::,,...............,,::.,,,,:,::,,:,:,,,:,;:
,.::,:,,,,,;;;;;;;;r;;::,..............................;;;:;::::,:::::::,:,:,,,
: ,,:,,,,,,,,,,,,,:;rrr;;:;,,,,,,,::,.,.:.,.,;s,:;;;;:;:;;;;;::::,:::,:::,:,:,:
,.,,,,,,,...,,.,,....................................:,............:,,,:,:,,,,,
Net: <ethaddr> not set. Reading from E-fuse
Detected MACID:0:18:31:88:37:82
DaVinci EMAC
Hit any key to stop autoboot: 3 2 1 0
mmc1 is available
reading boot.scr
440 bytes read
Running bootscript from MMC/SD to set the ENV...
## Executing script at 80900000
reading uImage
2372948 bytes read
***** Kernel: /dev/mmcblk0p1/uImage *****
***** RootFS: /dev/mmcblk0p2 *****
## Booting kernel from Legacy Image at 81000000 ...
Image Name: Linux-2.6.37-ga3643b9
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2372884 Bytes = 2.3 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
<5>Linux version 2.6.37-ga3643b9 (root@svn) (gcc version 4.4.0 (GCC) ) #1 Fri Feb 1 17:02:05 MSK 2013
CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: ti8168evm
Linux version 2.6.37-ga3643b9 (root@svn) (gcc version 4.4.0 (GCC) ) #1 Fri Feb 1 17:02:05 MSK 2013
CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: ti8168evm
<6>bootconsole [earlycon0] enabled
bootconsole [earlycon0] enabled
<6>reserved size = 0 at 0
reserved size = 0 at 0
Memory policy: ECC disabled, Data cache writeback
Memory policy: ECC disabled, Data cache writeback
<5>Truncating RAM at 90000000-bfffffff to -afffffff (vmalloc region overlap).
Truncating RAM at 90000000-bfffffff to -afffffff (vmalloc region overlap).
<6>OMAP chip is TI8168 1.1
OMAP chip is TI8168 1.1
<7>On node 0 totalpages: 173568
<7>free_area_init_node: node 0, pgdat c04afffc, node_mem_map c04ed000
<7> Normal zone: 1728 pages used for memmap
<7> Normal zone: 0 pages reserved
<7> Normal zone: 171840 pages, LIFO batch:31
<7>pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
<7>pcpu-alloc: [0] 0
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 171840
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 171840
<5>Kernel command line: mem=166M@0x80000000 mem=768M@0x90000000 console=ttyO2,115200n8 earlyprintk androidboot.console=ttyO2 root=/dev/mmcblk0p2 rw rootfstype=ext3 rootdelay=1 init=/init ip=off
Kernel command line: mem=166M@0x80000000 mem=768M@0x90000000 console=ttyO2,115200n8 earlyprintk androidboot.console=ttyO2 root=/dev/mmcblk0p2 rw rootfstype=ext3 rootdelay=1 init=/init ip=off
<6>PID hash table entries: 4096 (order: 2, 16384 bytes)
PID hash table entries: 4096 (order: 2, 16384 bytes)
<6>Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
<6>Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
<6>Memory:Memory: 166MB 166MB 768MB 768MB = 934MB total
= 934MB total
<5>Memory: 682276k/682276k available, 11996k reserved, 0K highmem
Memory: 682276k/682276k available, 11996k reserved, 0K highmem
<5>Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
vmalloc : 0xf0800000 - 0xf8000000 ( 120 MB)
lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
modules : 0xbf000000 - 0xc0000000 ( 16 MB)
.init : 0xc0008000 - 0xc0036000 ( 184 kB)
.text : 0xc0036000 - 0xc0473000 (4340 kB)
.data : 0xc0474000 - 0xc04b55c0 ( 262 kB)
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
vmalloc : 0xf0800000 - 0xf8000000 ( 120 MB)
lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
modules : 0xbf000000 - 0xc0000000 ( 16 MB)
.init : 0xc0008000 - 0xc0036000 ( 184 kB)
.text : 0xc0036000 - 0xc0473000 (4340 kB)
.data : 0xc0474000 - 0xc04b55c0 ( 262 kB)
<6>SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
<6>NR_IRQS:375
NR_IRQS:375
<6>IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
<6>Total of 128 interrupts on 1 active controller
Total of 128 interrupts on 1 active controller
<6>GPMC revision 6.0
GPMC revision 6.0
<4>Trying to install interrupt handler for IRQ368
Trying to install interrupt handler for IRQ368
<4>Trying to install interrupt handler for IRQ369
Trying to install interrupt handler for IRQ369
<4>Trying to install interrupt handler for IRQ370
Trying to install interrupt handler for IRQ370
<4>Trying to install interrupt handler for IRQ371
Trying to install interrupt handler for IRQ371
<4>Trying to install interrupt handler for IRQ372
Trying to install interrupt handler for IRQ372
<4>Trying to install interrupt handler for IRQ373
Trying to install interrupt handler for IRQ373
<4>Trying to install interrupt handler for IRQ374
Trying to install interrupt handler for IRQ374
<3>Trying to install type control for IRQ375
Trying to install type control for IRQ375
<3>Trying to set irq flags for IRQ375
Trying to set irq flags for IRQ375
<6>OMAP clockevent source: GPTIMER1 at 27000000 Hz
OMAP clockevent source: GPTIMER1 at 27000000 Hz
Console: colour dummy device 80x30
Console: colour dummy device 80x30
<6>Calibrating delay loop... Calibrating delay loop... <c>986.31 BogoMIPS (lpj=4931584)
986.31 BogoMIPS (lpj=4931584)
<6>pid_max: default: 32768 minimum: 301
pid_max: default: 32768 minimum: 301
<6>Security Framework initialized
Security Framework ini<6>mmc0: new high speed SDHC card at address b368
mmc0: new high speed SDHC card at address b368
<6>mmcblk0: mmc0:b368 USD 3.72 GiB
mmcblk0: mmc0:b368 USD 3.72 GiB
<6> mmcblk0: p1 p2 p3
mmcblk0: p1 p2 p3
<6>EXT3-fs: barriers not enabled
EXT3-fs: barriers not enabled
<6>kjournald starting. Commit interval 5 seconds
kjournald starting. Commit interval 5 seconds
<6>EXT3-fs (mmcblk0p2): EXT3-fs (mmcblk0p2): using internal journalusing internal journal
<7>ext3_orphan_cleanup: truncating inode 8148 to 0 bytes
<6>EXT3-fs (mmcblk0p2): EXT3-fs (mmcblk0p2): 1 truncate cleaned up1 truncate cleaned up
<6>EXT3-fs (mmcblk0p2): EXT3-fs (mmcblk0p2): recovery completerecovery complete
<6>EXT3-fs (mmcblk0p2): EXT3-fs (mmcblk0p2): mounted filesystem with writeback data modemounted filesystem with writeback data mode
VFS: Mounted root (ext3 filesystem) on device 179:2.
VFS: Mounted root (ext3 filesystem) on device 179:2.
<6>devtmpfs: mounted
devtmpfs: mounted
<6>Freeing init memory: 184K
Freeing init memory: 184K
<4>init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_score_adj instead.
init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_score_adj instead.
<3>init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'
init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'
# <3>init: untracked pid 56 exited
init: untracked pid 56 exited
<3>init: untracked pid 57 exited
init: untracked pid 57 exited
syslink: disagrees about version of symbol module_layout
syslink: disagrees about version of symbol module_layout
pvrsrvkm: disagrees about version of symbol module_layout
pvrsrvkm: disagrees about version of symbol module_layout
omaplfb: disagrees about version of symbol module_layout
omaplfb: disagrees about version of symbol module_layout
vpss: disagrees about version of symbol module_layout
vpss: disagrees about version of symbol module_layout
<3>init: untracked pid 69 exited
init: untracked pid 69 exited
ti81xxfbpvrsrvkm: disagrees about version of symbol module_layout
pvrsrvkm: disagrees about version of symbol module_layout
omaplfb: disagrees about version of symbol module_layout
omaplfb: disagrees about version of symbol module_layout
<3>init: untracked pid 85 exited
init: untracked pid 85 exited
<3>init: untracked pid 87 exited
init: untracked pid 87 exited
<3>init: untracked pid 99 exited
init: untracked pid 99 exited
<3>init: untracked pid 98 exited
init: untracked pid 98 exited
pvrsrvkm: disagrees about version of symbol module_layout
pvrsrvkm: disagrees about version of symbol module_layout
omaplfb: disagrees about version of symbol module_layout
omaplfb: disagrees about version of symbol module_layout
<3>init: untracked pid 102 exited
init: untracked pid 102 exited
<3>init: untracked pid 112 exited
init: untracked pid 112 exited
<3>init: untracked pid 113 exited
init: untracked pid 113 exited
pvrsrvkm: disagrees about version of symbol module_layout
pvrsrvkm: disagrees about version of symbol module_layout
<3>init: untracked pid 115 exited
init: untracked pid 115 exited
omaplfb: disagrees about version of symbol module_layout
omaplfb: disagrees about version of symbol module_layout
<3>init: critical process 'servicemanager' exited 4 times in 4 minutes; rebooting into recovery mode
init: critical process 'servicemanager' exited 4 times in 4 minutes; rebooting into recovery mode
<6>musb-hdrc musb-hdrc.1: remove, state 1
musb-hdrc musb-hdrc.1: remove, state 1
<6>usb usb2: USB disconnect, address 1
usb usb2: USB disconnect, address 1
<7>usb usb2: rpm_resume flags 0x4
<7>usb usb2: rpm_resume returns 1
<6>musb-hdrc musb-hdrc.1: USB bus 2 deregistered
musb-hdrc musb-hdrc.1: USB bus 2 deregistered
<6>musb-hdrc musb-hdrc.0: remove, state 1
musb-hdrc musb-hdrc.0: remove, state 1
<6>usb usb1: USB disconnect, address 1
usb usb1: USB disconnect, address 1
<7>usb usb1: rpm_resume flags 0x4
<7>usb usb1: rpm_resume returns 1
<6>musb-hdrc musb-hdrc.0: USB bus 1 deregistered
musb-hdrc musb-hdrc.0: USB bus 1 deregistered
<0>Restarting system with command 'recovery'.
Restarting system with command 'recovery'.
Best regards,
Anton