Hi,
I want to connect two EVMs (DSP TMS320C6678) with a BOCS http://processors.wiki.ti.com/images/0/00/DualEVM_BOC_quick_setup_guide_09SEPT13.pdf
And I have a question about the Power supply:
should I elect the thow EVMs (12Volts) or just once???
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I want to connect two EVMs (DSP TMS320C6678) with a BOCS http://processors.wiki.ti.com/images/0/00/DualEVM_BOC_quick_setup_guide_09SEPT13.pdf
And I have a question about the Power supply:
should I elect the thow EVMs (12Volts) or just once???
Hi,
According to the BOC user's guide each board is normally powered by it's own +12V power supply.
IV. EVM Power Source [16, 17, 18]
Traditionally the EVM’s installed into the Boc will have there own power supplies
Hi,
thank you very much,
Now I want to connect tow EVMs(DSPTMSc6678) via the BOC with communication PCI express,
I maked the configuration by default of the jumpers (User guide, section II), but in section XVI. (Common PCI e REFCLK Source) indicates others things!!
how can I do this communication PCIe??
Hi,
The configuration by default of the jumpers mentioned in the BOC's User Guide Insure the communication PCIe between EVMS or there are others configuration that I should do??
Thank's