Other Parts Discussed in Thread: AM3874
Hi,
Our customer will use 1.8V Oscillator to DEV_OSC input of AM3874. But they can't find any oscillator with 1.8V output. Could you recommend some oscillator with 1.8V output for AM3874?
They are trying to make an Oscillator. But they can't make it because they don't have soem specification is needed. The needed specification is the below.
* Input capacitance value(pF)
* Accuracy of the frequency - 50ppm , Should it be included the change over the years?
* VIH, VIL value
* The specific condition for Duty min45%, max 45% - the spec of voltage level
* Tr, Tf value and specific condition (voltage level 10%, 90% ?)
* Some restricted condition for AM3874. - 1.8V power supply is input to the both AM3874 and the oscillator at same time. Is this timing allowed by AM3874?
I appreciate your quick reply.
Best regards,
Michi