HI all
We are trying to use simulink's embedded coder to generate code for the OMAP L137/TMS320C6747 board.
The problem is the lack of configuration on the ADC block. We need to set which channel (Mic-in or line-in) to select, and we need to use both channels simultaneously for our audio project.
The ADC block for the C6713 DSK in embedded coder allows the user to chose ADC source (with mic boost) which is our main problem, sampling rate etc. The ADC block of the C6747 board lacks many of these parameters.
Is there an update or a package for more configuration options? Why does this newer board have less configuration???
Without Simulink, we have been trying to learn to code but this board also does not have a tutorial like the C713 does and we are novice at best at programming. We have been stuck for two weeks.
please help!