This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

continuous mode YUV sensor at 720p60

Hi,

   I have a YUV sensor which can give 720P@60 at UYVY format.  I want to use Dm36x Resizer at continuous mode to resize UYVY 720P@60 frame  to 420:SP 720P@60 and encode it . It works in single shot mode. But I do not want to use single shot mode as it is having overload problems.

Is it possible to use Dm36x Resizer at continuous mode for  UYVY input format?

Regards,

Mahendra Kumar A.G.