Can someone point out the cause of the error, I have encountered and corrected URL errors, this one I am not too sure of.
NOTE: package expat-2.0.1-r1: task do_fetch: Started
NOTE: package expat-2.0.1-r1: task do_fetch: Succeeded
NOTE: Running task 343 of 427 (ID: 164, /home/hirst689/oe/oe-layersetup/sources/oe-core/meta/recipes-core/dbus/dbus_1.4.16.bb, do_fetch)
NOTE: package dbus-1.4.16-r4.0-arago1: task do_fetch: Started
NOTE: package dbus-1.4.16-r4.0-arago1: task do_fetch: Succeeded
NOTE: Running task 344 of 427 (ID: 163, /home/hirst689/oe/oe-layersetup/sources/meta-arago/meta-arago-extras/recipes-extended/thttpd/thttpd_2.25b.bb, do_fetch)
NOTE: package thttpd-2.25b-r0-arago0: task do_fetch: Started
NOTE: package thttpd-2.25b-r0-arago0: task do_fetch: Succeeded
NOTE: Running task 345 of 427 (ID: 162, /home/hirst689/oe/oe-layersetup/sources/oe-core/meta/recipes-graphics/freetype/freetype_2.4.9.bb, do_fetch)
NOTE: package freetype-2.4.9-r0-arago0: task do_fetch: Started
NOTE: package freetype-2.4.9-r0-arago0: task do_fetch: Succeeded
NOTE: Running task 346 of 427 (ID: 161, /home/hirst689/oe/oe-layersetup/sources/meta-openembedded/meta-oe/recipes-core/jpeg/libjpeg-turbo_svn.bb, do_fetch)
NOTE: package libjpeg-turbo-8d+1.2.1-r4: task do_fetch: Started
WARNING: Failed to fetch URL svn://libjpeg-turbo.svn.sourceforge.net/svnroot/libjpeg-turbo;proto=http;module=trunk
ERROR: Fetcher failure: Fetch command export HOME="/home/hirst689"; export SSH_AGENT_PID="1214"; export SSH_AUTH_SOCK="/tmp/keyring-WjoM1a/ssh"; export GIT_CONFIG="/home/hirst689/oe/oe-layersetup/build/arago-tmp-external-arago-toolchain/sysroots/x86_64-linux/etc/gitconfig"; export PATH="/home/hirst689/oe/oe-layersetup/build/arago-tmp-external-arago-toolchain/sysroots/x86_64-linux/usr/bin/armv7a-vfp-neon-oe-linux-gnueabi:/home/hirst689/oe/oe-layersetup/build/arago-tmp-external-arago-toolchain/sysroots/am335x-evm/usr/bin/crossscripts:/home/hirst689/oe/oe-layersetup/build/arago-tmp-external-arago-toolchain/sysroots/x86_64-linux/usr/sbin:/home/hirst689/oe/oe-layersetup/build/arago-tmp-external-arago-toolchain/sysroots/x86_64-linux/usr/bin:/home/hirst689/oe/oe-layersetup/build/arago-tmp-external-arago-toolchain/sysroots/x86_64-linux/sbin:/home/hirst689/oe/oe-layersetup/build/arago-tmp-external-arago-toolchain/sysroots/x86_64-linux//bin:/home/hirst689/arago-2011.09/armv7a/bin/:/home/hirst689/ti-sdk-am335x-evm-05.06.00.00/linux-devkit/bin/:/home/hirst689/oe/oe-layersetup/sources/oe-core/scripts:/home/hirst689/oe/oe-layersetup/sources/bitbake/bin:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/home/hirst689/oe/oe-layersetup/sources/oe-core/scripts"; /usr/bin/env svn co -r 837 http://libjpeg-turbo.svn.sourceforge.net/svnroot/libjpeg-turbo/trunk@837 trunk could not be run:
None
ERROR: Function failed: Fetcher failure for URL: 'svn://libjpeg-turbo.svn.sourceforge.net/svnroot/libjpeg-turbo;proto=http;module=trunk'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/hirst689/oe/oe-layersetup/build/arago-tmp-external-arago-toolchain/work/armv7a-vfp-neon-oe-linux-gnueabi/libjpeg-turbo-8d+1.2.1-r4/temp/log.do_fetch.21294
NOTE: package libjpeg-turbo-8d+1.2.1-r4: task do_fetch: Failed
ERROR: Task 161 (/home/hirst689/oe/oe-layersetup/sources/meta-openembedded/meta-oe/recipes-core/jpeg/libjpeg-turbo_svn.bb, do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 346 tasks of which 304 didn't need to be rerun and 1 failed.
Summary: 1 task failed:
/home/hirst689/oe/oe-layersetup/sources/meta-openembedded/meta-oe/recipes-core/jpeg/libjpeg-turbo_svn.bb, do_fetch
Summary: There were 2 WARNING messages shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.
hirst689@hirst689-laptop:~/oe/oe-layersetup/build$