This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

gst-launch & gst-inspect problem on 8168 DVRRDK

Hi,

     I am using the gstreamer in 8168 DVRRDK_02.00.00.23, and copied the folder "DVRRDK_02.00.00.23\ti_tools\linux_devkit\arm-none-linux-gnueabi\usr\bin" & folder "DVRRDK_02.00.00.23\ti_tools\linux_devkit\arm-none-linux-gnueabi\usr\lib" and gst-plugin-scanner to target nsf system.

   Then, I set the export variables in following:

              export LD_LIBRARY_PATH=/lib:/lib/gstreamer-0.10

              export GST_PLUGIN_PATH=/lib:/lib/gstreamer-0.10

              export GST_PLUGIN_SYSTEM_PATH=/lib:/lib/gstreamer-0.10

              export GST_PLUGIN_SCANNER=/lib:/lib/gstreamer-0.10

 

Then I executed the following command:

                ./gst-launch -v filesrc location=sample.264 ! 'video/x-h264' ! h264parse access-unit=true ! omx_h264dec ! omx_scaler ! omx_ctrl display-mode=OMX_DC_MODE_1080P_60 ! omx_videosink sync=false

 

However, I failed & and got the following debug info:

      (gst-launch-0.10:958): GStreamer-WARNING **: External plugin loader failed. This

 most likely means that the plugin loader helper binary was not found or could n

ot be run. If you are running an uninstalled GStreamer setup, you might need to

update your gst-uninstalled script so that the GST_PLUGIN_SCANNER environment va

riable gets set.

 

Memory usage summary: heap total: 0, heap peak: 0, stack peak: 0

         total calls   total memory   failed calls

 malloc|          0              0              0

realloc|          0              0              0  (nomove:0, dec:0, free:0)

 calloc|          0              0              0

   free|          0              0

Histogram for block sizes:

 

(gst-launch-0.10:958): GStreamer-WARNING **: Failed to load plugin '/lib/libthre

ad_db-1.0.so': /lib/libthread_db-1.0.so: undefined symbol: ps_lgetfpregs

 

(gst-launch-0.10:958): GStreamer-WARNING **: Failed to load plugin '/lib/libterm

cap.so': /lib/libtermcap.so: file too short

 

(gst-launch-0.10:958): GStreamer-WARNING **: Failed to load plugin '/lib/libncur

ses.so': /lib/libncurses.so: ELF file version does not match current one

 

(gst-launch-0.10:958): GStreamer-WARNING **: Failed to load plugin '/lib/libncur

sesw.so': /lib/libncursesw.so: ELF file version does not match current one

WARNING: erroneous pipeline: no element "h264parse"

 

Could you tell me what is the problem.