Other Parts Discussed in Thread: SYSBIOS
Hi
I have a legacy project that was developed using CCS 5.1 and Code Generation Tools 7.2.4. The target is a TCI6618 DSP and we use SYSBIOS 6.
When I build this project with CCS 5.2 or 5.3 the application crashes. The crash happens when a function returns that is called from main(), i.e. before any tasks are created. Here is the console output:
A0=0x0 A1=0x30002a80
A2=0x15000000 A3=0x0
A4=0x1844004 A5=0x0
A6=0x400 A7=0x30
A8=0x1 A9=0x1844018
A10=0x81bb04 A11=0x81bb00
A12=0x8f3700 A13=0x513d28
A14=0x8f34ac A15=0x8f3680
A16=0x80 A17=0x30002a80
A18=0x400 A19=0x30002800
A20=0x81ba34 A21=0x81ba38
A22=0x81ba28 A23=0x81ba30
A24=0x0 A25=0x0
A26=0xc0 A27=0x81ba2c
A28=0x0 A29=0x81ba54
A30=0x34 A31=0x893dd8
B0=0x0 B1=0x50100
B2=0x855dd4 B3=0x0
B4=0x1 B5=0x4
B6=0x30003a80 B7=0x2640100
B8=0x1000 B9=0x1000
B10=0x8404032 B11=0x2020000b
B12=0xa0352024 B13=0xc01804
B14=0x894f68 B15=0x8952f4
B16=0x3521c000 B17=0x5
B18=0x30002b80 B19=0x3521a000
B20=0x4900c13a B21=0x6842
B22=0x24204008 B23=0x4050
B24=0xe890192 B25=0x40aed4f1
B26=0x40020900 B27=0x8c2
B28=0x400401 B29=0x2600045
B30=0x810021ac B31=0x3fff
NTSR=0x0
ITSR=0x1000c
IRP=0x8100246c
SSR=0x0
AMR=0x0
RILC=0x0
ILC=0x0
Exception at 0x8100246c
EFR=0x2 NRP=0x8100246c
Internal exception: IERR=0x8
Opcode exception
ti.sysbios.family.c64p.Exception: line 248: E_exceptionMin: pc = 0x8100246c, sp = 0x008952f4.
xdc.runtime.Error.raise: terminating execution
I don't know how to determine the reason for the crash. Could it be simply that the stack space is too small? Does the console output tell you anything that I am missing? I would appreciate some advice for how to fix this please.
Best regards
David