This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Android recovery disabled

Hi

As per the link mentioned below, patch has been released to disable the recovery until new mechanism:

http://e2e.ti.com/support/omap/f/849/t/220553.aspx?pi70913=1

So has the new mechanism been implemented?  Can it be integrated with ICS.

Are there any flaws with the original recovery mechanism.

  • You can try the links in next post, they reported that recovery was working.

    http://e2e.ti.com/support/omap/f/849/p/243001/851295.aspx

  • Hi Manuel

    Thanks for looking into the issue.

    The link which you are referring to is posted by us only, we are able to bring up the recovery by making changes to bootable/recovery/default_recovery_ui.c

    Actually my query was, why the recovery is disabled in JB. Also the link which I mentioned earlier indicates that a new mechanism for recovery is being implemented, so just wanted to know about that.

    Hope I am interpreting it correctly.

  • In the post that I indicate and where it is mentioned about alternate JB procedure, it was expected that it worked in JB and I was providing instructions for ICS. Customer was using JB and he reported that it worked.

    One of the changes between JB and ICS is that in JB it is using .cpp code, after running a comparative there were some differences that are indicated in the post but mainly it was the same code with a different interface that was functional. There were 2 solutions, both include changes from the document obtained from TI representative, one solution was including the changes from omapedia.org about recovery and Blaze but applied to JB and .cpp, the second was the change mentioned by the Customer about the same.

    About the mechanism to be implemented I think it was about recovery for Blaze Tablet, the one for Blaze was ok and can be used instead.

  • Directly recover SMS from Android Mobile Phone, you must to use a 3rd data recovery for Android.

    Android SMS Recovery Software is powerful that directly recover deleted or lost SMS text messages due to delete or format the SD card, restoring factory settings, etc from Android. This software support most of Android phones and tablets like Samsung, HTC, LG, Motorola, Sony,Huawei, ZTE, ect and keep data on your device original, no risk, deletion, modification or personal information leaking.

    How to Restore Lost Data from Android Micro SD Cards