We are using a Micron MT48LC2M32B2P-6 64M (512K x 32 x 4 BANKS) SDRAM on the EMIFB interface; this SDRAM is capable of 167MHz. We are presently running this part at 150 MHz and are only using this external SDRAM for initialization. Our question is two part. 1) Is there a maximum speed for the EMIFB interface? This part is 32 bit wide and we only have one SDRAM on the PCB. 2) Also, we are concerned that the 150 MHz clock runs continuously and we would like to turn off the clock after initialization is complete (especially because of premature aging on the present rev of this DSP).