Other Parts Discussed in Thread: UCD9222, UCD7242, UCD74111, UCD74120, TMS320C6670
Hi,
I am currently designing my board which has two DSPs in which the CVDD is supplied by UCD9222 and UCD7242.
Due to the 10A limitations of the UCD7242, I am looking at using UCD74120 or the UCD74111.
May I know if there are any reference designs to connect up the UCD74120 with UCD9222 to supply voltage for the C6678?
Regards,
Allan