Hi
When i was connected beaglebone board with my Host PC via minicom utility. After reset the board it starts booting and at the end it asks for login password(beaglebone login:). Writing password as root, then no beagle prompt will be Open(i.e nothing will be happens). Minicom version=2.5
Message in terminals in the booting process:
U-Boot SPL 2011.09-00053-gb423c52 (Aug 10 2012 - 11:26:55)
Texas Instruments Revision detection unimplemented
No daughter card present
No AC power, disabling frequency switch
OMAP SD/MMC: 0
reading u-boot.img
reading u-boot.img
U-Boot 2011.09-00053-gb423c52 (Aug 10 2012 - 11:26:55)
I2C: ready
DRAM: 256 MiB
WARNING: Caches not enabled
No daughter card present
NAND: HW ECC Hamming Code selected
No NAND device found!!!
0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
*** Warning - readenv() failed, using default environment
Net: cpsw
Hit any key to stop autoboot: 0
SD/MMC found on device 0
reading uEnv.txt
33 bytes read
Loaded environment from uEnv.txt
Importing environment from mmc ...
Loading file "/boot/uImage" from mmc device 0:2 xxa2
3489560 bytes read
## Booting kernel from Legacy Image at 80007fc0 ...
Image Name: Angstrom/3.2.34/beaglebone
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3489496 Bytes = 3.3 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
XIP Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
systemd-fsck[60]: Angstrom-Cloud9-: clean, 79331/218592 files, 373217/873534 blo
cks
[ 7.450317] musb_g_ep0_irq 720: SetupEnd came in a wrong ep0stage setup
.---O---.
| | .-. o o
| | |-----.-----.-----.| | .----..-----.-----.
| | | __ | ---'| '--.| .-'| | |
| | | | | |--- || --'| | | ' | | | |
'---'---'--'--'--. |-----''----''--' '-----'-'-'-'
-' |
'---'
The Angstrom Distribution beaglebone ttyO0
Angstrom v2012.05 - Kernel 3.2.34
beaglebone login:root
Cursor is continuously blinking and no further communication with my host PC
Please reply