This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LCDK Omap L138 ethernet between boards

Other Parts Discussed in Thread: OMAPL138

Hello, 

I want to read data from ethernet-I send data from my PC (for example ping ipaddress) I and want to read this in my program. I use enet_echo example from OMAPL138_StarterWare_1_10_03_03. My code:

int main(void)
{
unsigned char macArray[6] = MAC_ADDRESS;
unsigned int ipAddr;

/* Set up the UART2 peripheral */
UartSetUp();

/* Set up the pin multiplex for EMAC and MDIO and enable PSC */
EMACPinMuxSetup();
PSCModuleControl(SOC_PSC_1_REGS, HW_PSC_EMAC, PSC_POWERDOMAIN_ALWAYS_ON,
PSC_MDCTL_NEXT_ENABLE);

EMACIntrSetUp();

/* Initialze the lwIP library, using DHCP.*/
#if STATIC_IP_ADDRESS

ipAddr = lwIPInit(0, macArray, STATIC_IP_ADDRESS, 0, 0, IPADDR_USE_STATIC);

#else

ipAddr = lwIPInit(0, macArray, 0, 0, 0, IPADDR_USE_DHCP);

#endif


IpAddrDisplay(ipAddr);

LocatorConfig(macArray, "evmAM1808 enet_lwip");

/* Initialize the sample echo server. */
echo_init();

/* Loop forever. All the work is done in interrupt handlers. */
while(1)
{
; /* Perform nothing */
}
}

/*
** Interrupt Handler for Core 0 Receive interrupt
*/
static void EMACCore0RxIsr(void)
{

//HERE I THINK I SHOULD READ DATA
int p;
 p=(EMAC_RXCP(0)); //DOESNT WORK


#ifdef _TMS320C6X
IntEventClear(SYS_INT_EMAC_C0RX);
#else
IntSystemStatusClear(SYS_INT_C0_RX);
#endif
lwIPRxIntHandler(0);
}

Generally I want to send data through ethernet between two lcdk boards omap l138. 

I can see EMAC and MDIO registers but nothing changes when I send ping IP from my PC. It should be?

 

Mark