This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to enable all frequencies for BeagleBoard-xM in Sitara Linux

Other Parts Discussed in Thread: DM3730

Hi,

I am wondering how to enable all frequencies for the BeagleBoard-xM using Sitara Linux, as the frequencies shown in /sys/devices/system/cpu/cpu0/cpufreq/scaling_available_frequencies only show 300000 600000 800000 , whereas the DM3730 inside the BBxM supports 1 GHz as well.

I imagine it is because the distribution may only have been designed for BeagleBoard (no xM). Is there a way to include the extended frequencies?

Luis

  • Hi Luis,

    I recommend you to check the software which you are using whether is it built for the proper target. I checked the available frequences on my bouard and they are: 1000000 800000 600000 300000. The current frequence by default is 1000000.

    BR
    Tsvetolin Shulev