Other Parts Discussed in Thread: SYSBIOS
I'm having trouble trying to set up caching from DDR3 to the L2. I've selected under the "Available Products" pane SYS/BIOS > Target Specific Support > C66 > Cache ("Use Cache"). When I open the Cache module, there is nothing listed below. Shouldn't there be some configuration settings?
I also have configured the platform file for L1P 32K, L1D 32K, L2 64K, and Code: L2SRAM, Data: L2SRAM, Stack: L2SRAM.
I'm running an FFT on data stored in DDR3, but it is very slow (~2Million Cycles at 1GHz). I imagine this is because I'm not caching accross L2, but maybe there's another problem.
What am I doing wrong?
Ryan