This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem booting C6748 using nand 16

Other Parts Discussed in Thread: OMAP-L138

Hi,

We are trying to boot our program on 6748 without success.  A sligtly modified version of the code boots well on our other device using c6745 and nand8.  

We would need so help to make this work.

I genereted the code using aisgen for D800k008 using D800k006 device and nand16 option. I programed the code into flash with the nand writer application in debug.  

Using the diagnostic Gel file, I Obtained this:

C674X_0: Output: Target Connected.
C674X_0: Output: ---------------------------------------------
C674X_0: Output: Memory Map Cleared.
C674X_0: Output: ---------------------------------------------
C674X_0: Output: Memory Map Setup Complete.
C674X_0: Output: ---------------------------------------------
C674X_0: Output: PSC Enable Complete.
C674X_0: Output: ---------------------------------------------
C674X_0: Output: PLL0 init done for Core:200MHz, EMIFA:25MHz
C674X_0: Output: DDR initialization is in progress....
C674X_0: Output: PLL1 init done for DDR:126MHz
C674X_0: Output: Using DDR2 settings
C674X_0: GEL Output: 13 bit row address
C674X_0: Output: DDR2 init for 126 MHz is done
C674X_0: Output: ---------------------------------------------
C674X_0: Output: EMIFA Pins Configured for NAND.
C674X_0: Output: ---------------------------------------------
C674X_0: GEL Output: ---------------------------------------------
C674X_0: GEL Output: | BOOTROM Info |
C674X_0: GEL Output: ---------------------------------------------
C674X_0: GEL Output: ROM ID: d800k006
C674X_0: GEL Output: Silicon Revision 2.0
C674X_0: GEL Output: Boot pins: 16
C674X_0: GEL Output: Boot Mode: NAND 16
C674X_0: GEL Output:
ROM Status Code: 0x0000001A
Description:C674X_0: GEL Output: NAND read page failed
C674X_0: GEL Output:
Program Counter (PC) = 0x8000F020

The device seems unable to read the flash.  We have successfully read/writted in flash in our debug code so we know it works.  

The nand device is MT29F4G16ABADAWP.

Is there a known issue with the nand 16 device in boot mode ?

thank you.