This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Also, I missed this part of the fatal error.. Might be important to mention as well.
[63563.804565] ------------[ cut here ]------------
[63563.809570] WARNING: at arch/arm/mach-omap2/omap_l3_smx.c:161 omap3_l3_app_irq+0xe4/0x130()
[63563.818511] In-band Error seen by USB_OTG at address 0
[63563.824096] Modules linked in: libertas_sdio cdc_acm
[63563.829498] [<c0012134>] (unwind_backtrace+0x0/0xe0) from [<c0037c20>] (warn_slowpath_common+0x4c/0x64)
[63563.839599] [<c0037c20>] (warn_slowpath_common+0x4c/0x64) from [<c0037cb8>] (warn_slowpath_fmt+0x2c/0x3c)
[63563.849914] [<c0037cb8>] (warn_slowpath_fmt+0x2c/0x3c) from [<c0023ac8>] (omap3_l3_app_irq+0xe4/0x130)
[63563.859924] [<c0023ac8>] (omap3_l3_app_irq+0xe4/0x130) from [<c007f68c>] (handle_irq_event_percpu+0x3c/0x21c)
[63563.870574] [<c007f68c>] (handle_irq_event_percpu+0x3c/0x21c) from [<c007f894>] (handle_irq_event+0x28/0x38)
[63563.881103] [<c007f894>] (handle_irq_event+0x28/0x38) from [<c00819fc>] (handle_level_irq+0xb4/0xc4)
[63563.890930] [<c00819fc>] (handle_level_irq+0xb4/0xc4) from [<c007f11c>] (generic_handle_irq+0x20/0x30)
[63563.900970] [<c007f11c>] (generic_handle_irq+0x20/0x30) from [<c000de54>] (handle_IRQ+0x60/0x84)
[63563.910461] [<c000de54>] (handle_IRQ+0x60/0x84) from [<c0417674>] (__irq_svc+0x34/0x78)
[63563.919067] [<c0417674>] (__irq_svc+0x34/0x78) from [<c001d658>] (omap3_enter_idle+0xf8/0x12c)
[63563.928344] [<c001d658>] (omap3_enter_idle+0xf8/0x12c) from [<c001d7f0>] (omap3_enter_idle_bm+0x164/0x1c0)
[63563.938720] [<c001d7f0>] (omap3_enter_idle_bm+0x164/0x1c0) from [<c0339040>] (cpuidle_idle_call+0xf0/0x26c)
[63563.949188] [<c0339040>] (cpuidle_idle_call+0xf0/0x26c) from [<c000e0b4>] (cpu_idle+0x44/0x94)
[63563.958465] [<c000e0b4>] (cpu_idle+0x44/0x94) from [<c05d16e4>] (start_kernel+0x250/0x294)
[63563.967315] ---[ end trace 0d8c0b4f212fe5d7 ]---