Hello,
We are working on TIDM8148EVM board.
We tested the encode application that's come with EzSDK on our EVM.
Regarding to rate control we get very limited results. For 720p input the minimum bitrate we are able to produce is ~0.8Mbps and for 480p it's ~1Mbps.
This means we are unable to set bit rate lower then this, it remains constant after the limit mentioned above.
For us these are very high minimum bitrates.
Can we configure bitrates lower then this? Is there any hardcoding inside encoder?