I have learned that the secure accelerator is for networking side of the features. Does the 66AK2E0x support secure boot? It means, if the code can be encrypted in the flash, and decrypt it when it's loaded into the DRAM.
Thanks,
John
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
John,
Secure Boot will be supported,
The technical documentation on it is still in progress, but will not be released on the external product page.
You will need to work with your local technical sales representative to get access to the Secure Boot documentation when it's available.
Please note that it will not be supported via the E2E forum, but through your local Field Applications Engineers.
Best Regards,
Chad