This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678 Memory Map

Hi guys,

I already got the logical memory map of the C6678 form SPRS691c and from http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/t/172296.aspx

But as I have understood this, it is only the memory map of the logical 32-bit Address space each CorePac sees (assuming default configuration of the XMCMPAX of each Core). But this logical address mapping is somehow worthless, if you change the address mapping using the XMC MPAX of the CorePac.

I wanted to make use of the XMCMPAC and to cofigure the remapping correctly I need to know the Memory map of the 36-Bit Address space of the C6678.

Is there any 36-Bit Memory Map available of the C6678? At which physical 36-Bit Address is for example the DDR3 memory?

Regards Fabian