This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Hawkboard support in Davinci Linux PSP 03.22.00.02



Hello,

I'm using OMAP L138 LCDK and gave a try to update to the latest linux psp 03.22.00.02.

In general it worked with the first limited tests, but I noticed I cannot use the SD card.

I looked into the kernel sources and found that arch/arm/mach-davinci/board-omapl138-hawk.c does not use CONFIG_HAWKBOARD_LCDK, and seems that it misses couple of other things too...

Is LCDK support planned in the later releases or is it better to stay with the kernel coming with the LCDK SDK (3.1.10)?

Thanks,

István