This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

compiler unable to get defined structure variable



my main program is, bffr.c  :

#include <stdio.h>

#include <stdlib.h>

#include <dsk6713.h>

 #include <dsk6713_aic23.h>

 #include "aic_32bit_io.h" #include "self_header.h"

 #include "tab.h"

 #include "CST2.h"

DSK6713_AIC23_CodecHandle hAIC23_handle;

union { Uint32 sample32bit; unsigned short sample[2]; }input;

CODSTATDEF  CodStat ;

PWDEF Pw;

//void Impls_respns_calc(float *ImpResp,float *PerLpc,float *QntLpc,PWDEF Pw); float fram[240],y[240],ssb_fram1[60],ssb_fram2[60], ssb_fram3[60],ssb_fram4[60]; float R_sbfrm1[12],R_sbfrm2[12],R_sbfrm3[12],R_sbfrm4[12],W_hns[60]; float a1[11][11]={{1},{1},{1},{1},{1},{1},{1},{1},{1},{1},{1}},a2[11][11]={{1},{1},{1},{1},{1},{1},{1},{1},{1},{1},{1}},a3[11][11]={{1},{1},{1},{1},{1},{1},{1},{1},{1},{1},{1}},a4[11][11]={{1},{1},{1},{1},{1},{1},{1},{1},{1},{1},{1}}; float p_est1,p_est2,f[240],lpc_a4[10],PrevLsp[10],CurrLsp[10],UnqLpc[40]; float Lsp[40],QntLpc[40],PerLpc[80],Dpnt[40],ImpResp[240],B=0.0,PrevErr[145]; Uint32 Rez; int L=0; //float p[6],q[6],p_d[6], q_d[6];

void main() {

int i;

my header file where i declare functions used in main file is , function.h :-

/* default functions used in self blocks */

 extern PWDEF Pw;

void FRMR();

 void HPF(float frm[], int n);

void SB_FRMR (float y_frm[], int n);

void LPC_anlys(float frm_ssb_fram1[],int s,float frm_ssb_fram2[],int n,float frm_ssb_fram3[],int o,float frm_ssb_fram4[],int p );

void PER_WEGTH_FLTL(float frm[],int n); void PITCH_ESTMTN(float x_f[], int m);

 void HRMNC_NSE_SHPNG(float x_f[],int a,float x_p_est1,float x_p_est2);

float LPCtoLSP_QNTN(float x_lpc_a4[],int a);

 void LSP_INQNTN(float *Lsp,float *PrevLsp,int LspId, Uint16 Crc);

void Lsp_Int(float *QntLpc ,float *CurrLsp, float *PrevLsp); void LsptoA(float *Lsp);

 void Impls_respns_calc(float *Impres,float *PerLpc,float *QntLpc,PWDEF Pw);

float Polynomial(float *Lpq, int CosPtr); float DotProd(float *in1,float *in2, int len);

the file where i defined constants and structures is , CST.h :-

/* harmonic noise shaping filter parameters */

typedef  struct   {    int   Indx;    FLOAT Gain;    } PWDEF;

but problem is that after rebuilding all these together in project i got error in all  lines of header file conntaing function declarations which uses PWDEF as undefined type.

i follow rules of ANSI C;

 

kindly help me to sort put this issue.