Other Parts Discussed in Thread: SYSBIOS
Hi ,
I wanted understand the use of MultiProc_getBaseIdOfCluster (). Is multiple c6678 chips (DSPC8681/8682)are required for clustering or within a single chip(EVM6678) can it be performed?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SYSBIOS
Hi ,
I wanted understand the use of MultiProc_getBaseIdOfCluster (). Is multiple c6678 chips (DSPC8681/8682)are required for clustering or within a single chip(EVM6678) can it be performed?
Hari,
Can you tell me what Library/Source base this is from? Maybe I can steer it in the correct direction, but I'm not familiar with that function.
Best Regards,
Chad
Hi Chad,
I am trying to write simple IPC code for 6678EVM ,in the one of examples of IPC, that function was used .I have enabled four cores and i grouped first two cores as one group(core 0 and core 1) and other two as another group (core 2 and core 3) i have assigned cluster ID as 0 to core0 and core 1 ,and cluster ID 2 for the core 2 ,core 3 in .cfg file
When i am debugging the cluster ID is zero for all the cores.
Regards,
Harikrishna
I got the answer ,it is for the multiple C6678's only..I got it in the sysbios IPC document only ..
Thanks for let us know. I thought it was BIOS related when you were referring to IPC in your follow up, so I had moved it to the BIOS forum.
-Chad