i use the CCS3 for the first.time.
Before continuing, i'm not good enough in english.
i wish to TMS320C6455 cpu process time before purchase DSP.
CCS3 setup and project create procedure are as below.
Please review it.
1. install CCS3
2. execute CCS3 Setup.exe
3. select C64xx CPU Cycle Accurate Simulator – TMS320C64xx – TMS320C6000
Processor Properties is default.
4. execute CCS3.exe
5. create New project.
6. add to source file, header file, rms6400.lib in project.
7. build project
8. load execute file(.out)
9. profile setup
10. run project
as a result, cpu process time of total FFT2D is 2.0sec.
it astonishes to believe.
image size is 128x128.
Please review about the wrong and left off the procedure and tell me your views.
Thanks.