This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to read time TCRR from DSP on DM814x

Section 23.3.10 of sprugz8c.pdf (TRM) states:

"So, to read the value of TCRR correctly, the first OCP read access has to be to the lower 16-bit
(offset = 28h), followed by OCP read access to the upper 16-bit (offset = 2Ah)"

Where do these 16-bit offsets magically come from? Are they in a table somewhere? Are they even correct?

Thanks,

Andrew