This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am3703 McBSP max bit clock



Hi,

according to the datasheet the max bit clock of McBSP in opp100 is high, 48MHz for  McBSP 1-4 and 32MHz for McBSP5.  So about 20ns and 31ns period.

But there is a wide range for the delay from the bit clock edge and frame/data valid on the tx side (0.6-14ns). This makes it impossible to meet to setup and hold timings on the receive side at full speed: even inverting the polarity of the bit clock on the rx side, the delay above is larger that half clock period. And we cannot work with a bit clock higher than 10-15MHz realistically.

Am I correct?
What is the reason for such a wide range for the "delay time, mcbsp_clkx actve edge to dx and fsx valid"?

Best regards
Massimo