This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x starter kit and USB Hub controller

Hi. I just bought the Starter Kit, and try get the develop system up and running.
I have created a virtual machine running Ubuntu, as described in dokomationen. I've  Installed CCS 5, and it run just fine.
But I can not connect to the target.
The host machine (Win 7) can not recognize AM335x, and therefore can not make it available for the virtuele machine.
When I look in properties for USB device it reads the Hardware ID as:

USB\VID_0428&2412&REV_0;;2

USB\VID_0428&2412


VID 0428 PID 2412 is the USB 2.0 Hub Controller USB2412 U16 on the PCB.
Can you help help with drive ? or what should I do ?

 I have tried to update the CCS on the host machine

 I have also tried to let the host machine find a driver on the net, without success.

Keld Kyllesbech