Other Parts Discussed in Thread: TPS51200
Hello.
Again, following TMDSSK3358, the pcb people took away the DDR3 VTT terminations with the two following arguments:
"One reason is that our DDR memory circuit is located near MCU and these resistors are needed if the routed trace length is over 6.3 cm. Other reason (found in Micron design guide) “The external parallel termination resistors that were required for DDR2 are no longer required with DDR3 JEDEC-compliant modules because the VTT terminating resistors are built onto the module”"
1) Does this seem to be ok?
2) If looking in AM335x datasheet figure 5.46 (DDR3 with termination) and figure 5.47 (DDR3 without termination) there seems to be some small change in the DDR_VREF circuitry. Now, we are using the TPS51200 as VTT Regulator according to SSK3358. But *if* the terminations are dropped, should we then need to make some change to the DDR_VREF circuitry provided from SSK3358?
Tnx