This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB Client



Hello,

I have developed a custom board DM8168 processor.
Is it possible to to USB client?
I want to use it to connect a custom board and PC.

Regards,

Hideki

  • Hi Hideki,

    I found several e2e threads stated that DM81xx USB to PC USB connection is possible. Check here:

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/t/140936.aspx

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/206026.aspx

    Regards,

    Pavel

  • Hi Pavel,

    Thanks for your answer.

    Please tell me that the rudimentary.

    I have read the TechnicalReferenceManual of DM8168.

    http://www.ti.com/lit/ug/sprugx8a/sprugx8a.pdf

    [24.1.2 Features Supported]

    ・Supports all modes of transfers (control, bulk, interrupt, and isochronous) in both host and device mode.

    ・Includes CDC Linux mode for accelerating CDC type protocols using short packet termination over
    USB.

    Q1.Is it the same meaning as "USB target controller" "device mode" is?

    Q1.Meaning of the same? "CDC type protocols" and "Communication Device Class"?

    Reagerd,

    Hideki 

  • Dear Hideki,

    Your assumptions are right.

    1. USB target controller and device mode is same. 

    2. CDC is used for communication device class.