This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Pandaboard ES GPIO Strange Behaviour !!

hello everyone,,

I'm working on a project using pandaboard es (OMAP4460) where i have to use one of the GPIO's as an output, but when i measure the values on any GPIO of the J3 expansion header, it gives me always 1.8 V even if, i didn't export this GPIO pin and the most strange also even if, this pin i configure it as input, IT STILL GIVES ME 1.8V, i tried to cat the value of this pin it gives me 0 but when measuring this pin with MM it gives 1.8V , and I also tried the MUX register for every gpio's pin and i make sure that's they are in mode 3 and are output_pin but still the pins give me 1.8 V !!?

I'm using ubuntu 12.04 pre-installed server image with u-boot as the bootloader,

it would be grateful, if anyone could help me with this issue !!

thanks in advance