Other Parts Discussed in Thread: TMS320C5515
I'm a test engineer with a CM and I have a customer that has a TMS320C5515 on their board with and external flash/sram combo device (AMI Semiconductor N04C1633E3BM) that is being pre-programmed. They have asked that we verify the CRC of the flash during In-Circuit Test (using an Agilent 3070). I do not have full access to the flash, so I have to go through the JTAG port on the TMS320C5515. Is there a software program and emulator/programmer that would be well suited to perform this request? We are also concerned with throughput times as we are building 1000s of boards a month.
Thanks,
Jon Roberts