Other Parts Discussed in Thread: SYSBIOS
Hi, everybody.
I'm using DM8148evm, CCS 5.2, and sys/bios 6.33.5.46.
I implemented console diagnostic mode task which is based on <stdio.h> console input and System_printf() console output.
The source code of this Diag_Task is as follows:
===============================================================================================
#include <ti/sysbios/knl/Task.h>
#include <xdc/runtime/System.h>
#include <stdio.h>
#include <stdlib.h>
Task_Handle DiagTask_Handle;
void Diag_Task()
{
char diag_cmd[15];
for(;;)
{
System_printf("C>:");
fgets(diag_cmd, sizeof(diag_cmd), stdin);
diag_cmd[strlen(diag_cmd)-1] = '\0';
fflush(stdin);
if(strcmp(diag_cmd, "Command1") == 0)
{
........
}
if(strcmp(diag_cmd, "Command2") == 0)
{
..........
}
} // for(;;)
}
========================================================================================
If I execute this program in CCS Jtag emulation mode, I can input string through console window.
However, interrupt service routine function is not called, when executing this program.
I setup the GPIO interrupt. If I delete the Diag_Task code, the ISR is called correctly.
Is is possible to receive CCS console input without halting system ?
How can I make the ISR called, while waiting the console input ?
Thank you.