This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM c6670 EMAC0 port Link not up

Connected the EVM 6670 board to the chasis. Able to power up the board. I am trying to send the network packet through EMAC0 port using the PA_emacExample project.

I tried to get the SGMII status for port 0 using CSL_SGMII_getStatus() call.  Here the link is not up due to that i am not able to initialize my emac port 0.

 

Is Init_SGMII required for EMAC0?

Is port 0 mac address is 00:01:02:03:04:05?

Is it possible to set the static IP address for the board? if yes how can i configure?

 

Thanks in advance.

 

Thanks & Regards,

K. Lakshmanan