Other Parts Discussed in Thread: TMS320C5515
Hello, I've CCS5 installed and I've the tms320c5515 evm. I created a new project for which I selected a DSP/BIOS example (clock example). It uses the GEL file from Spectrum Digital at startup and the code downloads neatly into the target using the debugger. But when I press 'run' everything crashes, even CCS5. I know the hardware and else is ok since I can run/debug any non Bios code. Would, of course, like to know waht I'm doing wrong or, failed to do.
k.rgds, Laurent