This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C66xx register access cycle



Hello,

I have been made to the benchmark test of SRIO on C667x.

I think it takes a long time to register access.

I measured the two registers in the following way.

 (PLL1 Setup for DSP @ 1000.0 MHz and 'data' was placed in the L2SRAM. )

**** old = TSCL;

data = *(volatile unsigned int*)0x02900D18;    <--- LSU1_REG6

now = TSCL; cycletime = now - old;

 

old = TSCL;

data = *(volatile unsigned int*)0x02900DE8;  <--- LSU_STAT_REG0

now = TSCL;

cycletime = now - old;

****

 

The result is as follows.  

 LSU1_REG6    register access cycle : 76 cycle  

 LSU_STAT_REG register access cycle : 113 cycle

 

So, I have a question, is this result reasonable ?

 

Best Regards,

Chi

 

  • Chi,

    Register are on a separate bus, which is a relatively slow bus as they are not accessed frequently.  That said, this does seem a little large.

    You should also determine the turnaround delay of performing the TSCL reads.

    old = TSCL;

    now = TSCL;

    Overhead = now - old.

    Then when you calculate the time, you can removed the overhead as well.