Other Parts Discussed in Thread: TVP5147M1, OMAP-L138
hallo,
I have OMAP L138 and I use DVSDK 04.03.00.06.
I have analog camera connected to L138 through TVP5147M1 (i have LogicPD Zoom OMAP-L138 EVM).
I want to take video stream from the camera and convert it in mpeg4 format using gstreamer.
I think that the command line should look like:
# gst-launch v4l2src device=/dev/video1 ! queue ! TIVidenc1 codecName=mpeg4enc engineName=codecServer iColorSpace=NV12 resolution=720x576 framerate=25 ! filesink location=movie.m4v -v
There are some details that I do not know, for example video4linux produce a stream in NV16 format, but mpeg4enc doesn't support it.
Can tou give me a command line example surely working, and the steps to get it works?
best regards