This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148 not booting when serial cable is connected

Hi,

The DM8148 EVM board boots fine from SD card when serial cable is not connected. But whenever I connect serial port and try to boot EVM, EVM is not booting. I'm seeing some corrupt data on minicom terminal which is not at all helpful. 

Is there anything I'm missing?

Following are some details about serial port setup:

Bps/Par/Bits : 115200 8N1

Hardware/Software Flow Control: No

Following is output I'm getting on minicom terminal:

Welcome to minicom 2.4

OPTIONS: I18n
Compiled on Jan 25 2010, 06:49:09.
Port /dev/ttyUSB0

Press CTRL-A Z for help on special keys

����������������������������������������������������������������������������|���
����������������������������������������������������+�����������������������|��
���������������������

Thanks,

Rajnikant