Other Parts Discussed in Thread: TMS320C6678
Hi folks
I am running DSPC-8681,which has four TMS320C6678.
for loading image, i am using PCIe interface as explained in the user manual and desktop linux sdk.
http://downloadt.advantech.com/ProductFile/Downloadfile1/1-M1Q98N/DSPC-8681E_UserGuide_0_6.pdf
that is working fine. but now I want load the image using ethernet boot mode, using a host application
I have some some questions:
Does it has ethernet boot mode support as tms320c6678 ?
If yes the how we can change the boot mode of DSPC-8681.?
if we can do do this using boot pins then what are the boot pin configuration to choose the ethernet boot mode.?
The defualt ibl is BIG endian or little. ?? If little than what is the procedure to flash the ibl on DSPC-8681E ??
as it uses the pci interface.?
Thanks
mw