Other Parts Discussed in Thread: OMAP-L138, OMAPL138
I'm trying to use the USB OTG port on the OMAP-L138 LCDK, using linux SDK. The USB1.1 interface will not work for my application. I'm not a driver expert but after sorting through the linux-3.1.10/arch/arm/mach-davinci/omapl138-hawk.c and various other files it doesn't appear to support OTG. Is there a driver available for the LCDK? If not, is there a driver that would be similar to LCDK that I could start with?
Any assistance would be appreciated.
Thanks,
Todd